3.1.4 Command line information

The character string of the command line of the assembler is output.

The output example of the command line information is shown below.

Command Line Parameter
a.asm -Xcommon=rh850 -Xprn_path      (1)

Number

Description

(1)

Character string of command line

The character string of the command line specified for the assembler is output.