The CC-RH supports the language specifications stipulated by the ANSI standards. These specifications include items that are stipulated as processing definitions. This section describes language specifications that are not specified or defined by the ANSI standard, or that are process-dependent.
It describes the differences between when the option for processing in strict compliance with the ANSI standard (-Xansi) is specified, and when it is not.
See "4.2 Extended Language Specifications" for extended language specifications explicitly added by the CC-RH.