4.1.1
Unspecified behavior
This section describes behavior that is not specified by the ANSI standard.
(1) | Execution environment - initialization of static storage |
Static data is output during compilation as a data section.
(2) | Meanings of character displays - final line location, backspace (\b), horizontal tab (\t), vertical tab (\t) |
This is dependent on the design of the display device.
(3) | Types - floating point |
IConforms to IEEE754Note.
Note | IEEE: Institute of Electrical and Electronics Engineers
IEEE754 is a system for handling floating-point calculations, providing a uniform standard for data formats, numerical ranges, and the like handled.
|
(4) | Expressions - evaluation order |
Unspecified.
(5) | Function calls - parameter evaluation order |
Unspecified.
(6) | Structure and union specifiers |
See "(8) Bit field" for the boundary alignment of structure objects with bit fields.
(7) | Function definitions - storage of formal parameters |
Unspecified.
Unspecified.