Divides the value of the 1st term of an expression by the value of its 2nd term and returns the integer part of the result.
Divides the value of the 1st term of an expression by the value of its 2nd term and returns the integer part of the result.
The decimal fraction part of the result will be truncated. If the divisor (2nd term) of a division operation is 0, an error occurs
The result of the division "256 / 50" is 5 with remainder 6. |