Returns the value of the term as it is.
[Function]
Returns the value of the term of an expression without change.
[Application example]
(1) | The value "5" of the term is returned without change.
The value "5" is defined in symbol "FIVE" with the .set directive.
|