5.3.3  
File input control instructions
 
Using the file input control instruction, the assembler can input an assembler source file or binary file to a specified position.
The following file input control instructions are available.
Table 5.16  | File Input Control Instructions  | 
 
| 
 | 
 | 
| 
 
INCLUDE 
 | 
 
Quotes a series of statements from another source module file 
 | 
| 
 
BINCLUDE 
 | 
 
Inputs a binary file 
 |