Assumes the contents of the binary file specified by the operand to be the result of assembling the source file at the position of this control instruction.  | 
This control instruction handles the entire contents of the binary files. When a relocatable file is specified, this control instruction handles files configured in ELF format. Note that it is not just the contents of the .text selection, etc. that are handled.  |