5.9 Description of Instructions

This section describes the instructions of the assembly language supported by the assembler.

For details of the machine instructions generated by the assembler, see the "Each Device User Manual".

 

 

 

Instruction

Indicates the meaning of instruction.

[Syntax]

Indicates the syntax of instruction.

[Function]

Indicates the function of instruction.

[Description]

Indicates the operating method of instruction.

[Flag]

Indicates the operation of flag (PSW) by the execution of instruction.

However, in (set1, clr1, not1) bit operation instruction, indicates the flag value before execution.

"---" of table indicates that the flag value is not changed.

[Caution]

Indicates the caution in instruction.