The following can be specified for disp:
Clears the bit specified by the first operand of the data indicated by the address specified by the second operand. The bits other than the one specified are not affected.
Clears the bit specified by the register value specified by the first operand of the data indicated by the address specified by the register value of the second operand. The bits other than the one specified are not affected.
Relative expression having $label for a label having a definition in the sdata/sbss-attribute section |
clr1 bit#3, HIGHW(value)[reg1] |
clr1 bit#3, HIGHW(value)[reg1] |
clr1 bit#3, LOWW(value)[reg1] |
clr1 bit#3, LOWW(value)[reg1] |
clr1 bit#3, HIGHW1(value)[reg1] |
clr1 bit#3, HIGHW1(value)[reg1] |
The clr1 machine instruction takes an immediate value in the range of -32,768 to +32,767 (0xFFFF8000 to 0x7FFF) as the displacement. |
If any of the following is specified as disp, the assembler executes instruction expansion to generate multiple machine instructions. |
Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section |
If a relative expression with #label or a relative expression with #label and with LOWW applied is specified as disp, [reg1] that follows the expression can be omitted. If omitted, the assembler assumes [r0] to be specified. |
If a relative expression with $label, or a relative expression with $label and with LOWW applied is specified as disp, [reg1] can be omitted. If omitted, the assembler assumes that [gp] is specified. |
If a relative expression with %label, or a relative expression with %label and with LOWW applied is specified as disp, [reg1] can be omitted. If omitted, the assembler assumes that [ep] is specified. |
The flag values shown here are those existing prior to the execution of this instruction, not those after the execution. |