The following can be specified for imm:
Subtracts the value of the register specified by the first operand from the value of the register specified by the second operand, and stores the result in the register specified by the third operand. If the result exceeds the maximum positive value of 0x7FFFFFFF, however, 0x7FFFFFFF is stored in the register specified by the second operand. Likewise, if the result exceeds the maximum negative value of 0x80000000, 0x80000000 is stored in the register specified by the second operand. In both cases, the SAT flag is set to 1
Subtracts the value of the absolute expression or relative expression specified by the first operand from the value of the register specified by the second operand, and stores the result in the register specified by the second operand. If the result exceeds the maximum positive value of 0x7FFFFFFF, however, 0x7FFFFFFF is stored in the register specified by the second operand. Likewise, if the result exceeds the maximum negative value of 0x80000000, 0x80000000 is stored in the register specified by the second operand. In both cases, the SAT flag is set to 1.
Subtracts the value of the register specified by the first operand from the value of the register specified by the second operand, and stores the result in the register specified by the second operand. If the result exceeds the maximum positive value of 0x7FFFFFFF, however, 0x7FFFFFFF is stored in the register specified by the second operand. Likewise, if the result exceeds the maximum negative value of 0x80000000, 0x80000000 is stored in the register specified by the third operand. In both cases, the SAT flag is set to 1.
If the instruction is executed in syntax "satsub reg1, reg2" or "satsub reg1, reg2, reg3", the assembler generates one satsub machine instruction. |
If the instruction is executed in syntax "satsub imm, reg2", the assembler executes instruction expansion to generate one or more machine instructionsNote. |
If all the lower 16 bits of the value of imm are 0
Relative expression having !label or %label, or that having $label for a label having a definition in the sdata/sbss-attribute section |
satsub !label, reg |
satsubi !label, reg, reg |
satsub %label, reg |
satsubi %label, reg, reg |
satsub $label, reg |
satsubi $label, reg, reg |
Relative expression having #label or label, or that having $label for a label having no definition in the sdata/sbss-attribute section |
satsub #label, reg |
mov #label, r1 satsub r1, reg |
satsub label, reg |
mov label, r1 satsub r1, reg |
satsub $label, reg |
mov $label, r1 satsub r1, reg |
If the instruction is executed in syntax "satsub reg1, reg2" or "satsub imm, reg2", if r0 is specified as the second operand, the assembler outputs the following message and stops assembling. |