Pops from stack area (single register).
Pops the value of the register specified by the operand from the stack area.
When the pop instruction is executed, the assembler executes instruction expansion to generate two or more machine instructions. |
Instruction expansion is performed, and set via an add instruction. |