Memory comparison
[Classification]
Standard library
[Syntax]
#include <string.h>
int memcmp(const void *s1, const void *s2, size_t n);
[Return value]
An integer greater than, equal to, or less than 0 is returned, depending on whether the object indicated by s1 is greater than, equal to, or less than the object indicated by s2.
[Description]
This function compares the first n characters of an object indicated by s1 with the object indicated by s2.
[Example]
#include    <string.h> 
int func(const void *s1, const void *s2) {
        int i; 
        i = memcmp(s1, s2, 5);  /*Compares the first five characters of the character  
                                  string indicated by s1 with the first five  
                                  characters of the character string indicated by  
                                  s2.*/ 
        return(i); 
} 
 |