Memory copy
[Classification]
Standard library
[Syntax]
#include <string.h>
void    *memcpy(void *out, const void *in, size_t n);
[Return value]
Returns the value of out.  The operation is undefined if the copy source and copy destination areas overlap.
[Description]
This function copies n bytes from an object indicated by in to an object indicated by out.