This option checks the consistency of the address to which the section is allocated.
The consistency of the address to which the specified section is allocated is not checked.
This option checks the consistency of the address to which the section is allocated. |
The items that can be specified as type are shown below. |
Allocates the section to a fixed-address area (e.g. I/O area). If the address range overlaps with ROM or RAM, the setting for FIX is valid. |
Specify the start address and end address of the address range to check for consistency in hexadecimal as address1 and address2. |
The result is normal when section .text and section .bss are respectively allocated within the ranges from 0x100 to 0x1FF and from 0x200 to 0x2FF. |
If the -form={object|relocate|library} option, -strip option, or -device option is specified, this option will be invalid. |
If the -form={object|relocate|library} option, or -strip option is specified, this option will be invalid. |