This option checks the device file specified when creating an object file.
The device file is not checked.
This option checks that the device files specified when creating object files and the device file specified by the -device option are all the same. |
To check that the device files specified when creating object files and the device file specified by the -device option are all the same, describe as: |
If the -form={object|relocate|library} option or -strip option is specified, this option will be invalid. |