-S9


This option outputs the S9 record at the end.

[Specification format]

-S9

 

-

Interpretation when omitted

None

[Detailed description]

-

This option outputs the S9 record at the end even if the entry address exceeds 0x10000.

[Example of use]

-

To output the S9 record at the end, describe as:

>rlink a.obj b.obj -form=stype -output=c.mot -s9

[Remark]

-

If the -form=stype option is not specified, this option will be invalid.