This option extracts library modules.
To extract module "file1" from library file "lib.lib" and output it to a file with the object file output format, describe as: |
If the -form={absolute|hexadecimal|stype|binary} option and the -strip option is specified, this option will be invalid. |
When the -form={absolute|relocate|hexadecimal|stype|binary} option is specified, external symbols can be deleted. |