|
Same operation as when specified only one time (with no parameter)
|
-V, -help, -g, -far_rom, -goptimize, -pass_source, -signed_char, -signed_bitfield,
-volatile, -merge_string, -pack, -ansi, -refs_without_declaration, -large_variable,
-nest_comment, -check_language_extension, -Omerge_files,
-Ointermodule, -Owhole_program, -g_line
|
|
The parameters for all option specifications are valid
|
-D, -U, -I, -preinclude, -preprocess, -no_warning_num, -subcommand, -asmopt,
-asmcmd , -lnkopt, -lnkcmd
|
|
The last option specification and its location are valid, or the parameters for the last option specification are valid
|
-o, -obj_path, -asm_path, -prep_path, -O, -Oinline_level, -Oinline_size,
-Opipeline, -Ounroll, -Odelete_static_func, -Oalias, -Otail_call,
-Osame_code, -switch, -character_set, -stack_protector, -stack_protector_all,
-P, -S, -c, -use_mda, -memory_model, -dbl_size, -error_file, -misra2004,
-misra2012, -ignore_files_misra
|