If options are specified by the following combinations, an error will occur.
If the specifications in -cpu or -use_mda do not match the contents of the device file specified by -dev, an error will occur in the assembler.
A compile error will occur when -misra2004 and -misra2012 are specified simultaneously.