< Compile Options / Source Options >
Message output from the assembler or optimizing linkage editor cannot be controlled by this option. Message output from the optimizing linkage editor can be controlled by using the lnkcmd option to specify the message or nomessage option of the optimizing linkage editor. |