2.3.4 [E20]

Configure the operating environment on the Property panel below when using E20.

Caution

Only LPD communications are supported for communication with the target board.

Figure 2.36

Example of Property Panel [E20]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

2.3.4.1 [Connect Settings] tab

2.3.4.2 [Debug Tool Settings] tab

2.3.4.3 [Download File Settings] tab

2.3.4.4 [Flash Options Settings] tab

2.3.4.5 [Hook Transaction Settings] tab