Renesas Electronics
Configure the operating environment on the Property panel below when using Simulator.
Figure 2.51
Example of Property Panel [Simulator]
Follow the steps below by selecting the corresponding tab on the Property panel.
2.3.5.1 [Connect Settings] tab
2.3.5.2 [Debug Tool Settings] tab
2.3.5.3 [Download File Settings] tab
2.3.5.5 [Hook Transaction Settings] tab