2.3.5.1 [Connect Settings] tab

You configure the connection with the debug tool for each one of the following categories.

 

(1) [Clock]

(2) [Configuration]

(3) [CPU virtualization support function]

(1)

[Clock]

You can configure the clock.

Figure 2.52

[Clock] Category [Simulator]

(a)

[Main clock frequency [MHz]]

Specify the main clock frequency.

You can specify the frequency from the drop-down list or by directly entering a frequency value between 0.001 and 999.999 (unit: MHz) (default: [320.00]).

Caution

When the instruction simulator for RH850 is used, the CPU clock frequency will always be the same as the value of the main clock frequency set in this property.

(b)

[Select Timer/Trace clock frequency]

The clock frequency for using timer/trace function is displayed.

You cannot change the value of this property.

(c)

[Unit of Timer/Trace clock frequency]

The unit of the clock frequency for using timer/trace function is displayed.

You cannot change the value of this property.

(d)

[Timer/Trace clock frequency]

The value of the clock frequency for using timer/trace function is displayed.

Note, however, that "---_---" is displayed while disconnected from the debug tool.

You cannot change the value of this property.

(2)

[Configuration]

The property in this category is always disabled.

(3)

[CPU virtualization support function]

The property in this category is always disabled.