The program execution history can be collected only when a condition is met.
By setting a Point Trace event, the execution history is collected as trace data only when an arbitrary variable or I/O register is accessed with the specified type.
To use this function, follow the procedure described below.
2.12.4.1 Set a Point Trace event
2.12.4.3 Edit a Point Trace event [Full-spec emulator][E1][E20]