2.12.8 Search the trace data

To search for the collected trace data, click the button to open the Trace Search dialog box (note that the search is disabled during execution of a program).

In this dialog box, follow the steps below.

Note that by selecting the appropriate tab in this dialog box, you can choose to search for trace data at the instruction level or search at the source level.

Figure 2.120

Search Trace Data (Trace Search Dialog Box)

 

This section describes the following.

 

2.12.8.1 Search in the instruction level

2.12.8.2 Search in the source level