2.8 Execute Programs

This section describes how to execute programs.

Main operations in this section are taken place from the debug toolbar or the [Debug] menu in the Main window, where commands to control the execution of programs are included.

Caution

Items of the debug toolbar and the [Debug] menu are valid only while connected to the debug tool.

Remark

For "program execution control" for a microcontroller that supports multi-core, see also to "2.7 Select a Core (PE)".

Figure 2.79

Debug Toolbar (Floating State)

Figure 2.80

[Debug] Menu