2.3.3 [E1]

Configure the operating environment on the Property panel below when using E1.

Figure 2.23

Example of Property Panel [E1]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

2.3.3.1 [Connect Settings] tab

2.3.3.2 [Debug Tool Settings] tab

2.3.3.3 [Download File Settings] tab

2.3.3.4 [Hook Transaction Settings] tab