2.3.5 [EZ Emulator]

Configure the operating environment on the Property panel below when using EZ Emulator.

Figure 2.38

Example of Property Panel [EZ Emulator]

 

Follow the steps below by selecting the corresponding tab on the Property panel.

 

2.3.5.1 [Connect Settings] tab

2.3.5.2 [Debug Tool Settings] tab

2.3.5.3 [Download File Settings] tab

2.3.5.4 [Hook Transaction Settings] tab