You can edit an interrupt event which has already been set.
When editing, click the target interrupt event in the Events panel and select [Edit Condition] from the context menu. This will open the Detailed Settings of Interrupt Events dialog box [Simulator] in which you can edit the items. When finished, click [OK].
Directly enter a value between 1 and 16383.
The event will be encountered when the event conditions meeting the number of specified passages are satisfied.
You can edit an interrupt vector and the priority order. The procedure for editing is the same as that for [Interrupt event setting] tab [Simulator] in the Action Events dialog box (see "(1) Specify [Interrupt Vector]"and" (2) Specify [Priority]").