This dialog box is used to select a file-encoding.
This section describes the following.
From the [File] menu, open the Open File dialog box by selecting [Open with Encoding...], and then click the [Open] button in the dialog box. |
Select the encoding to be set.
The encoding of the selected file is selected by default.
Opens the selected file in the Open File dialog box using a selected file encoding. |
|
Not open the selected file in the Open File dialog box and closes this dialog box. |
|