2.3 Open Device Top View Panel

Open the Device Top View panel, where you can confirm the information entered for the pins of the microcontroller.

To open the Device Top View panel, double-click [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Top View] in the Project Tree panel.

Figure 2.6

Open Device Top View Panel

 

Remark

In the Property panel, on the [Pin Configurator Settings] tab, if "BGA" is selected for the Package type, then Device Top View panel cannot be opened.