This panel allows you to enter information on each pin of the microcontroller.
The Device pin list area area can be zoomed in and out by |
The following items are explained here.
On the Project Tree panel, double-click [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List]. |
On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List], and then press the [Enter] key. |
This area consists of the following buttons.
Displays the information in the Device pin list area in an expanded view. |
|
Displays the information in the Device pin list area in a folded view only. |
|
Clicks this button to automatically process the configuration information in the selected function, I/O, N-ch, and other fields after selecting one of the peripheral functions displayed in the first level on the [Macro] tab. |
|
Clicks this button to initialize the selected function, I/O, N-ch, and other fields after selecting one of the peripheral functions displayed in the first level on the [Macro] tab. |
|
Clicks this button to create an external peripheral controller from the external peripheral controller information on the [External Peripheral] tab, and display it in the Device Top View panel. |
|
Clicks this button to delete the information for the external peripheral controller displayed on the [External Peripheral] tab, on the first layer. |
Click the |
Click the |
This area displays the "device pin list" for entering information on the pins of the microcontroller.
Selecting the tab changes the order in which "information on each pin of the microcontroller" is displayed.
This panel has the following tabs:
This tab displays information on each pin of the microcontroller in the order of pin number.
This tab displays information on each pin of the microcontroller in the order it was grouped into peripheral functions.
This tab displays information about the pins connected to external peripherals in order grouped at the external-peripheral component level.