This tab displays information on each pin of the microcontroller in the order it was grouped into peripheral functions.
The following items are explained here.
On the Project Tree panel, double-click [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List]. |
On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List], and then press the [Enter] key. |
This area displays the device pin list for entering information on the pins of the microcontroller.
The device pin list in this area is organized in the order the pins were grouped into peripheral functions.
The following are the columns comprising the device pin list.
The following are the columns comprising the device pin list.
You cannot add information in the Macro Name, Total, Used, Used by other function, Pin Number, Pin Name, Description, Recommend Connection for Unused and Attention columns because they contain fixed information. |
If the Free in the Function column is changed to a specific pin name, color of the corresponding pin in the Device Top View panel changes from the color representing the unused pins to the color representing the used pins selected by clicking [Device Top View Settings] tab >> [Color] in the Property panel. |
To move columns (change the display order) in the device pin list, drag and drop the desired column to the desired location. |
To add the user's own column, use the New Column dialog box which opens by pressing the [New Column...] button in the Column Chooser dialog box which opens by pressing the |