debugger.CurrentConsumption.Enable


This function enables acquiring current consumption data.

If you run a program with this feature enabled, current consumption data will be acquired. [RL78/G13][Simulator]

[Specification format]

debugger.CurrentConsumption.Enable()

[Argument(s)]

None

[Return value]

If acquiring current consumption data was enabled successfully: True

If there was an error when acquiring current consumption data was enabled: False

[Detailed description]

-

This function enables acquiring current consumption data.

[Example of use]

>>>debugger.CurrentConsumption.Enable()
True
>>>