This function deletes a condition of performance measurement. [RH850][E1/E20/Full-spec emulator]
If the condition of performance measurement event was deleted successfully: True
If there was an error when deleting the condition of performance measurement event: False
This function deletes the condition of the performance measurement event number specified by performanceNumber. |
If performanceNumber is not specified, then conditions of all performance measurement event numbers will be deleted. |