[File Information] tab


This tab shows the detailed information on each file categorized by the following and the configuration can be changed.

 

(1) [File Information]

(2) [Notes]

Figure A.16

Property Panel: [File Information] Tab

[Description of each category]

(1)

[File Information]

The detailed information on the file is displayed and the configuration can be changed.

File name

The file name is displayed.

Change the file name on the project tree.

Default

file name

How to change

Changes not allowed

Relative path

The relative path from the project folder is displayed.

Default

The relative path from the project folder

How to change

Changes not allowed

Absolute path

The absolute path of the file is displayed.

Default

The absolute path of the file

How to change

Changes not allowed

Save with absolute path

Select whether to save the file location with the absolute path.

This property is not displayed if the Property panel being displayed while a dependency file is selected on the project tree.

Default

No

How to change

Select from the drop-down list.

Restriction

Yes

Saves the file location with the absolute path.

No

Saves the file location with the relative path.

Last update

The time and date on which this file was changed last is displayed.

Default

File updated time and date

How to change

Changes not allowed

Writable

Select whether to enable writing to the file.

This property is not displayed if the Property panel being displayed while a dependency file is selected on the project tree.

Default

Yes (when the file is write enabled)

No (when the file is not write enabled)

How to change

Select from the drop-down list.

Restriction

Yes

Enables the file to write.

No

Does not enable the file to write.

(2)

[Notes]

The detailed information on notes is displayed and the configuration can be changed.

This category is not displayed if the Property panel being displayed while a dependency file is selected on the project tree.

Memo

Add memos to the file.

Add one item in one line.

The specified memo is displayed as the subproperty.

Default

Memo[number of items]

How to change

Edit by the Text Edit dialog box which appears when clicking the [...] button.

For the subproperty, you can enter directly in the text box.

Restriction

Up to 256 characters

Up to 256 items can be specified.