|
R_TMR_KBm_BatchOverwriteRequestOn
|
Enables batch overwriting of the compare register.
Remark | The timing for batch-overwriting the content of the compare register is when a count value and a value set in the compare register are matched or an external trigger is generated after calling this API function. |
[Syntax]
void R_TMR_KBm_BatchOverwriteRequestOn ( void );
|
Remark | m is the unit number. |
[Argument(s)]
None.
[Return value]
None.