|
R_TMR_KBm_ForcedOutput_mn_Start
|
Enables input of the trigger signal used for the forced output stop function.
[Syntax]
void R_TMR_KBm_ForcedOutput_mn_Start ( void );
|
Remark | m is the unit number, and n is the channel number. |
[Argument(s)]
None.
[Return value]
None.