Below is a list of output file files by the Code Generator.
|
R_RTC_Set_ConstPeriodInterruptOn R_RTC_Set_ConstPeriodInterruptOff R_RTC_Set_CalendarCounterValue R_RTC_Get_CalendarCounterValue |
|||
|
R_SCIn_Serial_Multiprocessor_Send R_SCIn_Serial_Multiprocessor_Receive |
|||
*1 In case of [API output control] setting are default ([Output all API functions according to the setting]).
A:Output by settings on each peripheral functions panel automatically.