3.2.4
Linkage Map Information
The start and end addresses, size, and type of each section are output in the order of address. The following figure shows an example of linkage map information output.
*** Mapping List ***
(1) (2) (3) (4) (5)
SECTION START END SIZE ALIGN
P
00001000 00001000 1 1
C
00001004 00001007 4 4
D_2
00001008 000014dd 4d6 2
B_2
000014de 000050b3 3bd6 2
|
|
|
|
|
|
Section name
|
|
|
Start address
|
|
|
End address
|
|
|
Section size
|
|
|
Section boundary alignment value
|
Note | As the number for the alignment of code sections whose address is determined after linkage, when big endian is selected, a multiple of 4 is indicated regardless of the actual number for alignment at the time of compiling and assembling. |