The symbol reference information (cross-reference information) is output when -show=xreference is specified. The following figure shows an example of cross-reference information output.
*** Cross Reference List *** (1) (2) (3) (4) (5) No Unit Name Global.Symbol Location External Information 0001 a SECTION=P _func 00000100 _func1 00000116 _main 0000012c _g 00000136 SECTION=B _a 00000190 0001(00000140:P) 0002(00000178:P) 0003(0000018c:P) 0002 b SECTION=P _func01 00000154 0001(00000148:P) _func02 00000166 0001(00000150:P) 0003 c SECTION=P _func03 00000184 |
|
Unit number, which is an identification number in object units |
|
|
Symbol name output in ascending order of allocation addresses for every section |
|
|
Symbol allocation address, which is a relative value from the beginning of the section when -form=relocate is specified |
|
|
Address of an external symbol that has been referenced Output format: <Unit number> (<address or offset in section>:<section name>) |