2.5 Clear Analysis Information

By pressing the button located on the Toolbar on the Realtime OS Task Analyzer panel, the user can clear the analysis information that is displayed in the Child-panel display area.

Figure 2-9. Clear Analysis Information



Remark Pressing the button also clears the contents of the trace buffer.