2.6 Save Analysis Information
Where the task analyzer trace data is to be saved and the file name by which it is to be saved can be selected/specified on the
Save As dialog box which is opened when the
button is pressed.
Figure 2-10. Save As Dialog Box