2.4.4 On/Off of display of state lines and event marks
On the
Analysis Result panel, by pressing the
button located on the
Toolbar the user can select the type of state line to be displayed as an execution transition state for the processing program, and whether an event mark is or is not to be displayed as a real-time OS resource usage status, in the
Analysis information diagram area.
Figure 2-6. Chart Visualization Chooser Dialog Box
Remarks 1. Whether a state line and an event mark are or are not to be displayed can be specified by clicking on the applicable check box.