Renesas Electronics
top
with RI600V4
Analysis
FUNCTIONS
Open Analysis Result Panel
On/Off of item display
2.4.1 On/Off of item display
On the
Analysis Result panel
, using the
button located in the upper left corner of the
Analysis information table area
, the user can select types of items to be displayed as a CPU usage status in the table area.
To display or not to display a given item, use the
Column Chooser dialog box
that is opened by pressing the
button located in the upper left corner of the
Analysis information table area
.
Figure 2-3. Column Chooser Dialog Box
Remarks 1. Whether a given item is or is not to be displayed is specified by clicking on the applicable check box.
Checked
Displays the item in the
Analysis information table area
on the
Analysis Result panel
.
Not checked
Hides the item from the
Analysis information table area
on the
Analysis Result panel
.
2. Pressing the [Default] button in the
Column Chooser dialog box
resets the item types and their sorting order displayed in the
Analysis information table area
on the
Analysis Result panel
to their default condition.
Previous Topic
Open Analysis Result Panel
Next Topic
Filtering of analysis information
Table of Contents
On/Off of item display
Filtering of analysis information
Change of sort order
On/Off of display of state lines and event marks
Zoom in or out of execution transition display
Limiting range of usage status