Renesas Electronics
top
Build Tool Operation
FUNCTIONS
Overview
2.1 Overview
This section describes how to create a load module and user library.
Previous Topic
FUNCTIONS
Next Topic
Create a load module
Table of Contents
Overview
Create a load module
Create a user library
Use an existing GHS project file
Set the Type of the Output File
Set Compile Options
Set Assemble Options
Set Link Options
Set Create Library Options
Set Build Options Separately
Automatically Update the I/O Header File