This section describes how to use an existing GHS project file to create a new CS+ project.
You can use CS+ to debug load module files built by the GHS compiler, in the same manner as a debug-dedicated project. |
For notes on the use of GHS download-module files, refer to section "Advanced downloading" under "Download/Upload Programs" in chapter "FUNCTIONS" of "CS+ RH850 Debug Tool". |
The procedure for using an existing GHS project file to create a new CS+ project is shown below.
See "CS+ Integrated Development Environment User’s Manual: Project Operation" for details about (1), (4), (5), and (6). |
Create a new CS+ project, or load an existing one created using an existing GHS project file.
When you create a new project, specify [Using Existing GHS Project File(GHS CCRH850)] as the project type.
Confirm the setting of the [Path of Tools] category from the [Build Options] tab on the Property panel, and change it if this is required.
Set a GHS project file to be used in the [Build] category from the [Build Options] tab on the Property panel.
If you need to set build options, set them in the MULTI IDE from Green Hills Software in advance. |
Drag a load module file from Explorer or the like, and drop it onto the Download files node on the project tree.
For details, refer to section "Add a download file" under "Add a File to a Project" in chapter "USING AN EXTERNAL BUILD TOOL" of "CS+ Project Operation". In this case, read the statement "debug-dedicated project(s)" as "project(s) based on an existing GHS project file". |
If there are any commands you wish to run before or after the build process, on the Property panel, from the [Common Options] tab, in the [Others] category, set the [Commands executed before build processing] and [Commands executed after build processing] properties. |
Save the setting contents of the project to the project file.