R_OSTMm_Set_CompareValue


In interval timer mode, set start value of the down-counter.

In free-running comparison mode, set value for comparison.

[Syntax]

void    R_OSTMm_Set_CompareValue ( uint32 value );

Remark

m is the channel number.

[Argument(s)]

I/O

Argument(s)

Description

I

uint32 value;

Start value of the down-counter or comparison value

[Return value]

None.