Renesas Electronics
Below is a list of API functions output by the Code Generator for OS timer use.
Table 3.12
API Functions: [OS timer]
API Function Name
Function
R_OSTMm_Create
Performs initialization necessary to control the OS timer functions.
R_OSTMm_Create_UserInit
Performs user-defined initialization relating to the OS timer functions.
r_ostmm_interrupt
Performs processing in response to the OS timer interrupt.
R_OSTMm_Start
Start OS timer count.
R_OSTMm_Stop
Stop OS timer count.
R_OSTMm_Set_CompareValue
In interval timer mode, set start value of the down-counter.
In free-running comparison mode, set value for comparison.