r_dalin_callback_sendend


Performs processing in response to the DALI transmission end interrupt INTSTDLn.

Remark

This API function is called as the callback routine of interrupt process r_dalin_interrupt_send corresponding to the DALI transmission end interrupt INTSTDLn (performed when number of transmission data specified by R_DALIn_Send argument tx_num has been completed).

[Syntax]

static  void    r_dalin_callback_sendend ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.